FB#.LINEPITCH

Description

This parameter defines the line pitch for linear encoders in nm per line. This is only used when using linear motor types. For rotary motors, see FB.ENCLINES.

Context

See Feedback Settings and FB#.MECHTYPE.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

nm/line

Range

0.001 to 2000000.000

Default Value

20,000

Data Type

Integer

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported.